메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

SCI RXI Interrupts Not Generated

Last Updated:07/04/2018

Question:

SCI RXI interrupts are not generated. What could be the reasons and how to fix it?

Answer:

Please check the following items. 

(1)Make sure that ERI interrupts are not generated due to a reception error.  

(2)Check the ICU IEN register, IPR register, IR register, CPU "I" flag, and SCI SCR register. 

(3) Make sure that the SCI module stop bit is released.
 For products with the write protection function, release the write protection before writing the module stop bit.

(4)Make sure that the SCR.RIE/SCR.RE bit setting procedure is executed as described in the manual. 

(5) For products with MPC, it is necessary to set the PMR register of the IO port. For products without MPC, it is necessary to set the ICR register of the IO port. Please check the above register.

Suitable Products
RX Family
  • 이 기사가 도움이 되셨나요?