메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is the PLP period counted from the start of mass production of a product?

Latest Updated:04/01/2015

Question:

Is the PLP period counted from the start of mass production of a product?

Answer:

No, the PLP period is counted from the date that the product joins the program. Note that new products can only be added to the PLP after they have entered mass production.
Suitable Products
PLP (Product Longevity Program)
  • 이 기사가 도움이 되셨나요?