메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is the failure rate of each product listed somewhere?

Latest Updated:12/01/2006

Question:

Is the failure rate of each product listed somewhere?

Answer:

Since the failure rate varies depending on the temperature, power supply voltage, and other conditions, the failure rate (fit) for each product is not listed. To calculate the failure rate of a given product, refer to Chapter 2 and Chapter 5 of the Semiconductor Failure Rates information document. Chapter 2 explains the failure rate calculation procedure, and Chapter 5 lists the basic failure rates (λb) and the activation energy (Ea) of individual products.
For products that are not listed in this document, request the needed parameters through the seller of that product.
Suitable Products
  • 이 기사가 도움이 되셨나요?