메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there a recommended mount pad for surface mount diodes?

Latest Updated:08/01/2005

Question:

Is there a recommended mount pad for surface mount diodes?

Answer:

The pads differ depending on the package, so please go to the following Web site and click the mount pad for the relevant package.
Suitable Products
  • 이 기사가 도움이 되셨나요?