메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Marking part name on products

Latest Updated:08/01/2005

Question:

Marking part name on products

Answer:

The whole part name cannot be marked on small-size products, so the part name is indicated using a portion of the number or a symbol, etc.
An inspection symbol or manufacture code may also be marked in addition to the part name.
Suitable Products
  • 이 기사가 도움이 되셨나요?