메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Will products that aren't included in PLP be EOL in 10 years?

Latest Updated:04/01/2015

Question:

Will products that are not included in the Product Longevity Program (PLP) be EOL in 10 years?

Answer:

Products that do not meet the conditions to be a PLP product (FAQ No. 1010888) do not participate in the PLP. Note that products that are not published on the website and consumer products do not meet the conditions irrespective of their supply period. The production period of non-PLP products is determined based on the order situation and other factors. Thus, the supply period will not necessarily be less than 10 years.
Suitable Products
PLP (Product Longevity Program)
  • 이 기사가 도움이 되셨나요?