메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

(4559, 455A) Can operation of the voltage drop detection circuit be stopped?

Latest Updated:03/04/2005

Question:

(Low Voltage Detection/LVD)   Can operation of the voltage drop detection circuit be stopped? [2005/03/04]

Answer:

The voltage drop detection circuit cannot be stopped during MCU operation.
It can be stopped by going into RAM back-up mode. (#105068)
Suitable Products
4286
4571