메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

(7544) Should FFD4 to FFDAh data be deleted in the Mask ROM version ?

Latest Updated:01/25/2005

Question:

(ROM)  Regarding switching from one-time PROM version to Mask ROM version: Since the ID code check function is used in one-time PROM version, ID and other data are written into the ID code storage addresses (FFD4 to FFDAh). Should these data be deleted in the Mask ROM version ? [2005/01/25]

Answer:

It is not necessary to delete the data. (#104941)
Suitable Products
7544
  • 이 기사가 도움이 되셨나요?