메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

(H8/300H Tiny) When should I set the stack pointer?

Latest Updated:03/26/2009

Question:

When should I set the stack pointer?

Answer:

The first instruction of your program should set the stack pointer.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902
  • 이 기사가 도움이 되셨나요?