메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

(M32C) When reception is performed in UARTi, can TxDi pin used as an I/O port?

Latest Updated:09/22/2010

Question:

When only reception is performed using serial interface UARTi, can the TxDi pin used as an I/O port?

Answer:

By setting the function select register, the TxDi pin can be used as an I/O port.
Suitable Products
M32C/95
M32C/80
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80