메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Any precautions on using oscillation drive capacity High and Low?

Latest Updated:03/22/2012

Question:

Are there any precautions to be aware of when using the oscillation drive capacity "High" and "Low"?

Answer:

When switching the oscillation drive capacity of the main and sub clock between "High" and "Low", set the oscillation circuit parameters optimally in both conditions.
Please ask your oscillator manufacturer about the optimal oscillation circuit parameters on your system.
Suitable Products
M32C/95
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N
  • 이 기사가 도움이 되셨나요?