메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Are there any transmission enable/disable bits for SI/O3 and SI/O4?

Latest Updated:02/14/2006

Question:

Are there any transmission enable/disable bits for SI/O3 and SI/O4?

Answer:

No, there aren't any transmission enable/disable bits for SI/O3 or SI/O4. Transmissions are started by writing data to the SiTRR register.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/29
M16C/28
  • 이 기사가 도움이 되셨나요?