메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Buffer register value on H8S/2345 16bit Timer to general register ?

Latest Updated:03/23/2009

Question:

When is the value of the buffer register on the H8S/2345 16bit Timer transferred to the general register ?

Answer:

The value of the buffer register is transferred to the general register on a condition such as compare-match. Setting a value to the buffer register when the timer is stopped does not transfer the buffer to the general register at that time, it will occurat the next compare-match.
Suitable Products
H8S/2345
  • 이 기사가 도움이 되셨나요?