메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I use a higher resistance Crystal Oscillator?

Latest Updated:04/07/2011

Question:

In the Clock Pulse Generator section of the manual, the table Crystal Oscillator Characteristics shows max Rs resistance. Can I use a higher resistance Crystal Oscillator?

Answer:

The resistance value and capacitance value described in the table Characteristics of Crystal Oscillator are only for reference.
Please ask your oscillator's manufacturer for matching characteristics measurements and determine resistance and capacitance values based on that data.

 

Suitable Products
H8S Family
H8SX Family
  • 이 기사가 도움이 되셨나요?