메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I use alternative side of standard frequency of H8S/2134 subclock?

Latest Updated:03/23/2009

Question:

The standard frequency of the H8S/2134 subclock (EXCL) is 32.768 kHz. Can an alternative frequency be used ?

Answer:

Using another frequency other than 32.768 kHz is not tested and the subclock operation is not guaranteed.
Suitable Products
  • 이 기사가 도움이 되셨나요?