메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I use the WDT as an interval timer?

Latest Updated:03/24/2009

Question:

Can I use the WDT as an interval timer?

Answer:

No, you can't.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
  • 이 기사가 도움이 되셨나요?