메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can PMW be enable for channels that had 4 TGR registers using PWM mode 1?

Latest Updated:04/07/2011

Question:

In the timer pulse unit (TPU), can two different PWM outputs be enabled for a channel that has four TGR registers using PWM mode 1?

Answer:

Two different pins, TIOCA and TIOCC, are capable of PWM output. However, the output cycle will be the same because they share a counter.
To output PWM with a different cycle, please use a separate channel.

 

Suitable Products
H8S Family
H8SX Family