Can Renesas write in or read out code even code protection of QzROM is on?
Latest Updated:01/09/2009
Question:
(QzROM) When code protection of QzROM is enabled, although I can't write in or read out the code, is it possible for Renesas to write in or read out the code? Also, is there any way to unprotect it? [2009/01/09]
Answer:
When code protection of QzROM is enabled, even Renesas can neither write in/read out nor unprotect the code. (#107245)
Suitable Products
3803H |
3823 |
3850A |
3858 |
38D2 |
38D5 |
7544 |
7545 |
7546 |
7547 |
7548 |
7549 |