메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can Vcl pin on H8/3664F used for voltage on external peripheral device?

Latest Updated:03/18/2009

Question:

Can I use the Vcl pin on the H8/3664F to provide a constant voltage for an external peripheral device ?

Answer:

The Vcl pin is not actually a power supply but is used to attach an external stabilization capacitor for an internal step-down circuit. This pin is not capable of supply current to any external device.
Suitable Products
H8/300H Tiny