메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Do I have to keep the table area corresponding to unused interrupt free?

Latest Updated:04/01/2006

Question:

Do I have to keep the table area corresponding to unused interrupts free?

Answer:

No, you don't.
This memory area is reserved only for interrupts.
If you do not use an interrupt, the corresponding area can be used as a normal memory area.
Suitable Products
V850 Family