메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Do absolute maximum values eased during undershoot and overshoot?

Latest Updated:03/01/2005

Question:

(Electrical Characteristics)   Although the Absolute Maximum Ratings value for port input voltage is stated in the datasheet, I would like to know if the absolute maximum values are eased during short periods such as "undershoot" and "overshoot". [2005/03/01]

Answer:

The port input voltage should always be kept within the Absolute Maximum Ratings value stated in the datasheet, regardless of the duration the voltage is applied. (#104894)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549