Do you have any plans to support the block erase of M16C Flash Starter?
Latest Updated:02/14/2006
Question:
Currently, the M16C Flash Starter only supports a total erase. Do you have any plans to support the block erase?
Answer:
We don't have any plans to do this.
Suitable Products
R8C/18 |
R8C/19 |
R8C/1A |
R8C/1B |
R8C/10 |
R8C/11 |
R8C/12 |
R8C/13 |
R8C/14 |
R8C/15 |
R8C/16 |
R8C/17 |
R8C/20 |
R8C/21 |
R8C/22 |
R8C/23 |
R8C/24 |
R8C/25 |
R8C/26 |
R8C/27 |
R8C/28 |
R8C/29 |
R8C/2A |
R8C/2B |
R8C/2C |
R8C/2D |
R8C/32C |
R8C/33C |
R8C/34C |
R8C/35C |
R8C/36C |
R8C/38C |
R8C/3GC |
R8C/3JC |
R8C/32D |
R8C/33D |
R8C/35D |
R8C/3GD |
R8C/33T |
R8C/34E, R8C/34F, R8C/34G, R8C/34H |
R8C/36E, R8C/36F, R8C/36G, R8C/36H |
R8C/38E, R8C/38F, R8C/38G, R8C/38H |
R8C/L35C |
R8C/L36C |
R8C/L38C |
R8C/L3AC |
3803H |
3803L |
3850A |
38D2 |
38D5 |
M32C/87 |
M32C/86 |
M32C/85 |
M32C/84 |
M32C/83 |
M16C/80 |
M16C/62A |
M16C/62M |
M16C/62N |
M16C/62P |
M16C/6N4, M16C/6N5 |
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN |
M16C/30P |
M16C/29 |
M16C/28 |
M16C/26A |
M16C/26 |
M16C/1N |
M16C/6S |
EV5-ASIA (R0K3306S0D011BR) |
EV5-US (R0K3306S0D010BR) |
SDK-PLC-EU-A (or -B for CENELEC B band) |
M3A-0806 |