메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does DMA transfer takes first priority if request generated same time?

Latest Updated:03/15/2012

Question:

When a DMA request and an interrupt request are generated at the same time, does the DMA transfer always take first priority, regardless of the priority level of the interrupt?

Answer:

Because the DMAC has a higher priority than the CPU in the bus access, the DMA is always executed first. The interrupt is executed after the DMA transfer is completed.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A