메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does RTFI instruction generates a privileged instruction exception?

Latest Updated:04/01/2006

Question:

I am using T02 or T03 as the clock output for a serial interface.
Can I use the T02 or T03 output pin as a normal port?

Answer:

Even when timer 2 or timer 3 is used for the serial clock, TO02 or TO03 can be used as a normal port as long as timer output is not operated.
Suitable Products
V850 Family