메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does the BSY bit value changed when timer RH is set to stop counting?

Latest Updated:12/06/2013

Question:

When timer RH is set to stop counting (the RUN bit is set to 0), is the BSY bit value changed

Answer:

The BSY bit value remains unchanged.  Same applies to timer RE, and timer RE2.
Suitable Products
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx