메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does the QzROM version need to perform screening after programming?

Latest Updated:12/01/2005

Question:

(QzROM)  Does the QzROM version need to perform screening (baking as well as verification of programmed values) after programming ? [2005/12/01]

Answer:

No, it doesn't. (#105525)
Suitable Products
3803H
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549
  • 이 기사가 도움이 되셨나요?