메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

H8S/2357 DMA transfer word data from 8bit to 16bit access area?

Latest Updated:03/23/2009

Question:

Can the H8S/2357 DMA controller transfer word data from an 8bit access area to a 16bit access area?

Answer:

Its possible to transfer word data from 8bit access area to a 16bit access area. Select Word size transfer by setting the DMA control register (DMACR) DTSZ bit to 1.
Suitable Products
H8S/2398, 2357
  • 이 기사가 도움이 되셨나요?