메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How can I read the data written to internal flash memory?

Latest Updated:08/01/2001

Question:

How can I read the data written to internal flash memory?

Answer:

The contents written to the internal flash memory with a programmer cannot be read.
This is in order to protect the written program.

If it is absolutely necessary to read the program, consult your authorized NEC Electronics distributor.
In some cases, it may be possible to take the device to NEC Electronics and have its contents read.

Suitable Products
  • 이 기사가 도움이 되셨나요?