메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How can microcontroller recognize the mode in the uPD78F0034A?

Latest Updated:12/01/2011

Question:

In the uPD78F0034A, either 3-wire serial or UART can be used as the data transfer mode for programming.
How can the microcontroller recognize the mode?

Answer:

The mode is specified by the Vpp pulse count at the beginning of the flash programming mode.
For details, refer to section 6. Flash Memory Programming in the data sheet.
Suitable Products
  • 이 기사가 도움이 되셨나요?