메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I calcuate the case temperature of an IC?

Latest Updated:03/23/2009

Question:

How do I calcuate the case temperature of an IC?

Answer:

"The case temperature could be calculated with following formulas:

 

1:  Tj = Ta + Theta-ja x Q

2:  Tj = Tc + Theta-jc x Q

==>

3:  Tc = Ta + Theta-ja x Q - Theta-jc x Q

Ta       = ambient temperature

Tc       = case tempaerature

Tj       = junction temperature

Theta-ja  = thermal resistance junction-ambient

Theta-jc  = thermal resistance junction-case

Q        = power dissipation

e.g.

device: SH7709, SH7729

package: LQFP208-28x28-0.5 (Renesas code FP-208C)

Power dissipation: Q = 0,8 W

  Tc max = Ta max + (Theta-ja - Theta-jc) x Q

         = 85C  + (47C/W  - 7 C/W) x 0,8 W

         = 117 C"

Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B
  • 이 기사가 도움이 되셨나요?