메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I treat unused analog input pins on the SLP series ?

Latest Updated:03/18/2009

Question:

How do I treat unused analog input pins on the SLP series ?

Answer:

Please pull-up these unused pins by connecting a resistor of around 100k ohm between AVcc and the analogue input pin.
Suitable Products
H8 Family
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8/300L
H8 Super Low Power
  • 이 기사가 도움이 되셨나요?