메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How is the input for SCK designated? Is this setting made with PCR?

Latest Updated:03/26/2009

Question:

When using SCI, how is the input for SCK designated? Is this setting made with the port control register (PCR) corresponding to said pin?

Answer:

When using SCI, I/O designation at the SCK terminal is made with COM bit of the serial mode register (SMR) and CKE1 and CKE0 of the serial control register (SCR). It is not necessary to set the corresponding ports to PCR.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902