메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How much RAM capacity can users have?

Latest Updated:10/10/2006

Question:

How much RAM capacity can users use on what occasion(for example on on-chip debugging or writing on flash memory)?

Answer:

When you use the on-chip debugging and write on flash memory, there is no restrictions of RAM capacity for users to use, but program for on-chip debugging is stored in the 2KB area of flash memory only on the product with maximum flash memory capacity.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
  • 이 기사가 도움이 되셨나요?