메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to set up a system clock with 32MHz?

Latest Updated:03/26/2009

Question:

Please advise me how to set up a system clock. For instance, how can I set it up at 32MHz?

Answer:

It is suggested to set up PLL at x2 of input clock 16MHz for initial starting up. PLL is initially set up at x1after reset. All of setting of SCKCR register is for oesillator frequency.

For instance, if setting up bit 10 ~ 8 of SCKCR register at "010", system clock is same as oscillator freqeuncy.

Suitable Products
H8SX/1600
H8SX/1663
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622
H8SX/1500
H8SX/1580
H8SX/1544
H8SX/1520R
H8SX/1520
  • 이 기사가 도움이 되셨나요?