메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

If the ports are pulled up/down, is there a problem connecting to power?

Latest Updated:03/24/2009

Question:

When the ports are pulled-up or pulled-down, is there any problem if connecting port to power supply directly?

Answer:

Since it is possible that an over-current or under-current condition may occur in the event that the input protection circuit is damaged due to unexpected situations (such as variation of power supply voltage etc.), please connect a resistor between the power supply line and the pin.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power