메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

In the uPD78902x, can pull-up resistors be specified by a mask option?

Latest Updated:12/01/2011

Question:

In the uPD78902x, can pull-up resistors be specified by a mask option?

Answer:

Since all on-chip pull-up resistors for the ports of the uPD78902X are switched by software, no item is specified by mask option.
Suitable Products
UPD78902x
  • 이 기사가 도움이 되셨나요?