메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is 1.5mA an acceptable current while the DAi pin is outputting 0V?

Latest Updated:03/01/2005

Question:

(D/A Converter)  Is 1.5mA (peak) an acceptable current while the DAi pin is outputting 0V ? [2005/03/01]

Answer:

There is no problem with 1.5mA current flow itself. However, please keep in mind that D/A output precision will be greatly reduced while current is flowing. (#104838)
Suitable Products
3803H
3803L
  • 이 기사가 도움이 되셨나요?