메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is it OK not take action among INTIE2, STARTF and SLVRQ interrupts?

Latest Updated: 03/20/2017

Question:

During slave reception, I want the other communication party to perform retransmission, without performing reception (without overwriting RAM by DMA transfer).
To achieve this, I should not take any action upon occurrence of the INTIE2, STARTF, and SLVRQ interrupts: Is this an appropriate method?

Answer:

Yes, it is. However, be sure to clear the ISR flag.
Suitable Products
V850E2/Sx
V850E/Sx
V850ES/Sx