메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is memory mean one can't program after programming over minimum value?

Latest Updated:04/07/2011

Question:

Does the NWEC min value of internal flash memory rewrite number mean one cannot program after programming over the minimum value?

Answer:

No. You can program the internal flash memory over the NWEC minimum value (100 times), but the programming time (tP), erasing time (eE), total programming time (ΣtP), total erasing time (ΣtE), total programming/erasing time (ΣtPE) and data retain time (tDRP) characteristics will not be guaranteed.
Therefore, if you program over the NWEC minimum value, do not use the device in your end product.

 

Suitable Products
H8S Family
H8SX Family
  • 이 기사가 도움이 되셨나요?