메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there any documentation available concerning SMP foot pattern?

Latest Updated:08/05/2009

Question:

(Packaging)
Is there any documentation available concerning Surface Mount Package foot pattern? [2009/08/05]

Answer:

Please refer to the Renesas Semiconductor Package Mount Manual. -> here
Suitable Products
3803H
3803L
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549
  • 이 기사가 도움이 되셨나요?