메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there any problem that the oscillation amplitude is shown as approximately 1.5 V for the XIN-XOUT oscillation circuit?

Last Updated:12/26/2017

Question:

Is there any problem that the oscillation amplitude is shown as approximately 1.5 V for the XIN-XOUT oscillation circuit?

Answer:

The oscillation amplitude level of the XIN-XOUT oscillation circuit in the R8C/3x, Lx, and Mx Series is designed to be smaller than that in the R8C/1x and 2x Series to reduce current consumption.
There is no problem if the recommended oscillation circuit constant can be obtained by the matching evaluation from the oscillator manufacturer.
Suitable Products
R8C/3x
R8C/38A
R8C/Lx
R8C/Mx
  • 이 기사가 도움이 되셨나요?