메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Meaning of SSO output/input control in I/O Ports chapter

Latest Updated:10/05/2016

Question:

In the tables in the Programmable I/O Ports or I/O Ports chapter of the hardware manual, what do "SSO output control" and "SSO input control" mean?

Answer:

"SSO output control" and "SSO input control" refer to the TE bit and RE bit of the SSER register, respectively.
Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/3MK
R8C/34K
R8C/3MU
R8C/34U
R8C/3MQ
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
  • 이 기사가 도움이 되셨나요?