메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Output Data: Rewritten by interrupts while created before port

Latest Updated:12/07/2004

Question:

(Pin)   Could output data be rewritten by interrupts, etc. while it is being created before being output to a port? [2004/12/07]

Answer:

It depends the method by which the output data is created, but when processing data transiently using memory, a register and an accumulator, and rewriting them during an interrupt process without data retention, output data maybe rewritten. (#104913)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549
  • 이 기사가 도움이 되셨나요?