메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Ports P10-P15 (P10-P17 for 7549) set input mode; key-on for input to P10

Latest Updated:03/13/2008

Question:

(Interrupt)  Can ports P10 to P15 (P10 to P17 for 7549) be set to input mode and key-on wakeup enabled only for input to P10? [2008/03/13]

Answer:

Yes.
Key-on wake up settings for each individual pin can be enabled and disabled using the key input control register. (#106882)
Suitable Products
7548
7549
  • 이 기사가 도움이 되셨나요?