메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Read modify write

Latest Updated:08/01/2005

Question:

Read modify write

Answer:

This refers to a series of operations whereby the contents of memory cells or registers are read, the data is changed, and is then written.

Read modify write is performed for example to change the operation mode of a device by changing only the contents of a specific bit of a mode setting register and writing the changed data to the bit in question.

Suitable Products
  • 이 기사가 도움이 되셨나요?