메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Sometimes data is received incorrectly under the influence of noise.

Latest Updated:03/26/2009

Question:

Sometimes data is received incorrectly under the influence of noise. Is there any suggested countermeasure?

Answer:

Following product group can be evaluated by improved SCI module which has noise cancel circuit.
Suitable Products
H8/300H Tiny
H8/36109
H8/36049
H8/36912, H8/36902
  • 이 기사가 도움이 되셨나요?