메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What's the process if I want an A/D conversion equivalent circuit?

Latest Updated:03/01/2005

Question:

(A/D Converter)  I would like an A/D conversion equivalent circuit. [2005/03/01]

Answer:

Please refer to the information included in "CHAPTER 1. HARDWARE: FUNCTIONAL DESCRIPTION SUPPLEMENT" of the user's manual. (#104824)
Suitable Products
3803H
3803L
3850A
  • 이 기사가 도움이 되셨나요?