메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What's the status of P110-P115 to PWM outputs of TOM and TOU?

Latest Updated:03/22/2017

Question:

Regarding the PWM output disable function of the TOM timer and the TOU timer, what's the status of P110-P115 to PWM outputs of TOM and TOU?

Answer:

The ports (P110-P115) in relation to the TOM timer and the TOU timer always go to a high-impedance state no matter which mode they are in.
Suitable Products
32172, 32173
32180
32185
32186
32192
32195
32196