메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What frequency is required by the reference clock on a microcomputer?

Latest Updated:10/19/2004

Question:

(Clock)  What degree of precision in frequency is required by the reference clock on a microcomputer?
(calculation method only OK)
I would like to verify whether there will be any problem with the degree of stability of the external ceramic resonator I'm using to generate the reference clock. [2004/10/19]

Answer:

We do not have any specifications regarding clock frequency precision.
Normal MCU operation can be expected if oscillation meets the minimum main clock input cycle time and main clock input "H" ("L") pulse width described as timing requirements in electrical characteristics in the datasheet or user's manual.
Note that operation clock frequency precision influences the precision of timers, serial communication, etc. (#104908)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549
  • 이 기사가 도움이 되셨나요?