메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What frequency is the internal oscillator in Tiny series of devices ?

Latest Updated:03/26/2009

Question:

What is the frequency of the internal oscillator in the Tiny series of devices ?

Answer:

The frequency is not defined, the manual defines the minimum on chip overflow time and states a typical overflow period.
Suitable Products
H8/300H Tiny
  • 이 기사가 도움이 되셨나요?